This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Lithium Ion Battery Charger 975 watts

Hi,

The Charger Input Supply is AC, 170 V to 300 V, 50 Hz.

 

The Charger Output DC Supply is: 65 V DC +/- 0.50 V, and DC Output Charging Current at Max. 15.0 Amps +/- 0.3 Amp.

 

The acceptable Ripple on the Output DC Voltage is less than 1 V (Peak-to-Peak), at nominal rated Input of 230 Vac, 50 Hz.

Battery Charger Protections desired / required:

 A] Output Over-Load,

B] Output Short-Circuit,

C] Battery Terminals Reversal,

D] Output Over-Voltage,

E] Battery-Charger Circuit Over-Temperature.

Kindly suggest suitable device or solution or reference design for the above requirement

Regards

Atul Bhakay