This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24072: Not reaching max charging current at 5V

Part Number: BQ24072

Hi,

my BQ24072 it not reaching maximum charging current limits at 5V. I have it on a breadboard and connected to bench power supply with 2.5 A limit using the reference design, and these values:

CE -> low, TD -> low, TMR -> low, TS -> 10k, ILIM -> 1.3k, ISET -> 1.2k

And I try to charge LG 18650 cell with voltage around 3.5V.

When EN1 -> high, EN2 -> high, BA24072 operates without problem in suspend mode and des not consume more then 2 mA.

When EN1 -> low, EN2 -> low it draws at max 0.1 A as expected.

But when EN1 -> high, EN2 -> low with 5V at IN it charges the battery with only 0.3 mA if I rise the input voltage to around 6V then it reaches the limit of 0.5 A and charges the battery.

Same problem with configuration  EN1 -> low, EN2 -> high.

Any suggestions how to debug this or it is a normal behavior?

Thanks