Other Parts Discussed in Thread: UCC28070,
Greeting everyone.
I have been following this interesting thread.
I am also interested in using current sensor. My application is 24vdc input with 600W output in a tight package. I have a little trouble getting my head around a dc current transformer. It's a slightly different kind of magic. I can understand the volt-second balance and have used the Ion-Physics current transformers in the past.
I am looking t a 0.001 ohm current sense resistor with an amplifier on the output. The current transformer method looks like it might be worth looking at. I can keep the losses in the resistor to a couple of watt so I am interested to know what the current transformer approach will do for me.
You mentioned that the core must be reset. When commutating from a zero state to a power state the current always begins negative. Won't this automatically reset the core every half cycle? Would there be any benefit to using two cores - one for each source? Looks like the current is zero for a good part of the cycle. Or maybe one core with the source leads broken out and passed through the core in an anti-parallel fashion to drive core both ways?
Maybe there is enough strange magic here to prompt a short application note.
Thanks again.
Bob LaFrance