This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ34Z100: BQ34Z100 Design Procidure (Design Capacity, Design Energy settings and Golden Learning)

Part Number: BQ34Z100
Other Parts Discussed in Thread: EV2400

Along the same lines - I have some similar  questions regarding the BQ34z100:

 

1.      Can you provide us with an example golden file for the BQ34Z? The cell that we will be using is INR18650_F1L (Li-ion) and GP210AAHCB (NiMh), both cell data sheets are attached. Can you please check and confirm if you already have the Chem ID and the golden file for these cells?. If not, what is the process of getting the files?

2.      Does the Gauge require to do a calibration over time to main the SOC accuracy?, does it need host intervention?

3.      In the flags() status register, what action is expected from the host if the condition flag (CF) is set?

 

 

4.      The Rsense that we are currently using is 20mohm, is it OK or do we need to change it for better accuracy?

5.      Will it be possible to send me an eval kit for the EV2400 interface so I can monitor and configure the different values in the golden file?