This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
Regarding to inductor current mode on UCC28063, my customer is asking a question.
(Question)
Is DCM or CRM supported on this device?
It seems that there is only description of CCM on datasheet.
Just in case. I'm asking that.
Regards,
Tao 2199
Hi Tao2199,
UCC28063 is designed to operate in CRM mode. It is possible to enter DCM operation at very light load however.
Best Regards,
Ben Lough
Hello Ben,
Additional questions
(1) According to UCC28063 datasheet (page1),it seems that CCM is supported.(Below)
Is that wrong description? I’m confused ,and which is correct?
(2) About switching CRM and DCM on UCC28063.
Is principle same as UCC2056(UCC2805x)?
(Below: UCC2056 datasheet,page14)
Regards,
Tao 2199