This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools/TPS549D22: Thermal Simulation of IC-Die is lower than IC-TOP

Part Number: TPS549D22
Other Parts Discussed in Thread: TPS549B22, TPS548B22

Tool/software: WEBENCH® Design Tools

Hi TI Expert,

I'm using TI Webench to do some thermal simulation. Vin=12V, Vout=3.3V, Iout=23.5A, TI converter=TPS549D22

Per the simulation result, the IC Die temperature is lower than IC -TOP. It seems unreasonable. Suppose IC Die is the hottest spot. Could you help to explain the reason?

The Webench link is as below.

webench.ti.com/.../webench5.cgi

Thanks,

Dora