This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Team,
Please find the Circuit schematics of Battery management IC (BQ25601) enclosed within.
Request you to review the same and let us know your feedback.
Thanks and Regards,
Dear NIBIN,
The QON pin incorporates two functions to control BATFET.
1. BATFET Enable: A QON logic transition from high to low with longer than tSHIPMODE deglitch turns on BATFET and exit shipping mode.
One of the following events can also enable BATFET:
(1). Plug in adapter
(2). Clear BATFET_DIS bit
(3). Set REG_RST bit to reset all registers including BATFET_DIS bit to default (0)
2. BATFET Reset: When QON is driven to logic low by at least tQON_RST while adapter is not plugged in (and BATFET_DIS = 0), the BATFET is turned off for
tQON_RST. The BATFET is re-enabled after tBATFET_RST duration. This function allows systems connected to SYS to have power-on-reset.
Dear Naizeng Wang,
Instead of using a external switch for QON, can we take care of the shipment mode through software (Clear BATFET_DIS bit)?
After the shipped devices are received, what exactly need to be taken care in such case (through software, as there is no external switch).
Regards,
Nibin
Dear NIBIN,
When there is no external switch for QON, you can only exit shipping mode by plugging in adapter.
Reason:In shipping mode, the BATFET is disabled, so battery can't provide power for bq25601. If you don't provide power through adapter, the software won't work.
Nibin:
You can do either way. However, your system is usually supplied by SYS, so when the charger is in shipping mode, the host lost power and cannot communicate to the charger. In this case, you need to press QON button or plug in an adaptor.
When the BATFET is disabled (in shipping mode) and indicated by setting BATFET_DIS, one of the following
events can enable BATFET to restore system power:
1. Plug in adapter
2. Clear BATFET_DIS bit
3. Set REG_RST bit to reset all registers including BATFET_DIS bit to default (0)
4. A logic high to low transition on QON pin with tSHIPMODE deglitch time to enable BATFET to exit shipping
mode