Hi
iam using 14s32p battery pack. but while performing the short circuit test the various flags are ON mentioned below:
EUV
CUV
PV
cell 1 voltage 2000mV
cell 2 voltage 2000mV
But actual voltage of cell 1 and cell 2 is 3982mV & 3978mV. the remaining cell voltage is correct.
still i am able to communicate with the IC.
This is happens 4th times when due to short circuit test iam getting 2000mV then i need to change the IC.
But i am failed to understand why bq78pl116 unable to provide short circuit protection.
Even failed to achieve short circuit at 32 amps.