This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: WEBENCH® Design Tools
Hi! Ti E2E support,
My current company used UCC28070 as two phase interleave control for 800W PFC. I would like to ask TI whether TI has another controller which can have three interleave control for over 1000W PFC ( three phase more than two phase) in order to extend the current design into 1000W output power at least. (AC side input still is single phase)
In addition, I would like to know
1. whether new IC has boost "diode" control function or says if I use a MOSFET in replace the boost diode, the IC can run the FET (on high side).
2. Whether TI has controlled AC-DC rectifiers which basically using MOSFETs replace the rectified diodes in order to improve the system efficiency.
Looking to forwarding to your solutions!
Thanks,
Johnson Pi