Other Parts Discussed in Thread: OPT8241, CSD16301Q2, , SN74LVC2T45, TIDA-01573
We are developing indirect lidar and Direct lidar. I have some questions in terms of ti lidar components.
1. it is possible to get higher peak current when use gan and gate driver.
We aready reviewed your lidar evm board using opt8241 , 9221.
I want to get depth data for long distance. (12Mhz ~ upto 3Mhz , duty 50%)
So i try to change serveral below patrs . because I think gan is getting higher peak current than FET with gate driver.
- Gan(epc2040) instead of FET ( CSD16301Q2 )
- gate driver (Lmg1020) instead of sn74lvc2t45
Could you plz check my trial is proper or not for getting higher peak current .
2. how to get peak current in higher freqency and long duty using TIDA-01573.
As you mentioned in datasheet (TIDA-01573 ,figure3.) this driver can get 50A for 2ns.
But i need faster frequency and long duty cycle . ( 2M , 100ns, duty 20%)
If i lower temperature of laser enough, can i drive laser up to 50Apk ? what if i caculate peak current ? it's possible?
I think laser peak current is depend on duty cycle .
You can make any recomandation for our requirement (freq : 2M, pulse width : 100ns, duty 20%).
3. The way measure peak current of laser.
If i use detector ( thorlabs DET08C) and optical power meter ( Thorlabs PDA150A) .
Can i calulate peak power from measured power and proportion of laser.
Below list is light modulation information
duty : 20% / freq : 2M / LD Peak power : 40W
thank you.