This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC25630-1EVM-291: UCC256302 problem with Leakage inside Trans.

Part Number: UCC25630-1EVM-291


Hi-Ben san,

In the combination operation of PFC + LLC, the LLC transformer is self-made and replaced and the output transient characteristic of LLC is evaluated. When the load sudden change test of the maximum load (100%) ⇔ minimum load (0%) was carried out, the output reduction which occurred in the default state of the evaluation board previously was reproduced. In the previous inquiry, effective countermeasures could not be taken and a method to add dummy resistors to the output as the minimum load was taken but this time it can not be avoided, and for the investigation of the cause, the operation waveform of each part is observed again As a result, since unnatural waveforms were observed in principle, they are shown below. My original transformer is an internal leakage transformer.

As a result of the above results, the LL / SS terminal voltage sharply drops at the same timing and the FB terminal and VCR terminal voltage suddenly rise at any abnormal drop of the LLC output in any observation waveform, Since the load is in a light load state, there is no change in the load and it is judged as a static state in terms of the control response of the IC, but why such unsteady operation which is not logical occurs I do not understand.

In addition, there is little frequency of occurrence, it is a malfunction due to intrusion of noise into one of the terminals of the IC at a very irregular timing against repetition of sudden change in load, Can you think of entering more than one input terminal? Please teach this point.

Also, as an important point, this input varies greatly due to input bulk voltage fluctuation to the VCR pin (voltage divided by the resonance capacitor) during dynamic load fluctuation, and "VCR pin input voltage is less than 6 Vpp (absolute maximum The rating is 7 V) "in the UCC 256301 datasheet, section 8.2.2.19, is this maximum amplitude or 0 to peak value? It is to be worried that missing this can trigger a malfunction. (As you can see in the waveform when operating, it exceeds 7 V.)UCC256302 problem with Leakage inside Trans..pdf

  • Hi Doi-san,

    LL/SS will be discharged if the controller is detecting ZCS operation. If there is a great deal of noise on ISNS, this can create a false ZCS detection. Try populating C30 with ~220pF. Also please share the transformer specification of your custom transformer (Lm, Lr, turns ratio, etc).

    The controller look at the lower of LL/SS pin voltage and FBreplica to set the switching thresholds. If LL/SS is pulled low due to ZCS, this will push the LLC to higher switching frequency to get out of the capacitive region. When the switching frequency is pushed higher, this will also reduce the gain of the power stage, resulting in a dip in output voltage.

    VCR should always have a common mode voltage of 3V. Please keep the VCR waveform between 0V and 6V.

    Best Regards,
    Ben Lough
  • Hi Ben-san,

    Customer transformer is now tentative.

    Lm = 800uH

    Lr = 60uH  = 30uH (leakage) + 30uH (Added outside Inductor )

    Np = 48T,   Ns = 3T,  Nc = 4.5T 

  • Hi Doi-san,

    These parameters look fine. Please try populating C30 with ~220pF to see if this addresses the output voltage dropout issue.

    Best Regards,
    Ben Lough
  • Hi Ben-san,

    In the combination of PFC (UCC 28056) + LLC (UCC 256302)
    We are conducting output transient fluctuation test, but the following problem has come up.
    Please tell us about improvement measures.
     
    <Test condition>
    PFC input: AC 100 V
    LLC output: sudden change of 12 V 10 A (100%) ⇔ 0 A (0%)
    Load device: Electronic load
    Load sudden change cycle: 1 Hz duty = 50%
     
    <Problems>
    At the timing when the load has changed from 100% to 0%, the auxiliary power supply (Vcc) voltage by the LLC auxiliary winding of the evaluation board lowers and the IC operation instantaneously stops.
    After the operation is stopped, it restarts with the start circuit, but the 12 V output drops by several volts during this period. In case
    This failure phenomenon occurs at a considerable frequency.
    In case
    <Countermeasure and consideration>
    ① If 47 μF is added to the capacity of the smoothing capacitor C 16 = 120 μF of Vcc,
    The drop in Vcc was alleviated and some effect was recognized,
    Although the effect is not 100%, the drop frequency of 12 V output decreases.
     
    ② However, if this capacity 47 μF is added to the current circuit,
    The charging time of the start circuit becomes long, and it is not practical because the starting time from input power on to output rising is over.
     
    ③ As the output current range that maintains the output stability at present, the lower limit of the spec that can be compromised in sudden load change is around 0.3 A (3%), and it seems that it is necessary to add this dummy resistance.
    This will be designed to reverse from energy saving and high efficiency targets.
     
    ④ Consider setting the burst mode level for the above improvement.
    Based on the calculation formula of UCC 256304 Japanese version data sheet 8.2.2.21,
    To optimize the programming resistance and investigate whether the problem can be improved,
    Perform the following.
       When the voltage (upper limit: 1.86 V lower limit 1.14 V) measured by inserting the resistance 10 KΩ into the emitter of the photocoupler (U 2) was substituted into the calculation formula (75) of the data sheet,
    When calculated using IFb = 81 μA of the IC electrical characteristics table,
    The VLL value becomes a minus value, and the calculated numerical value has no validity, why?
     
    ⑤ From the contents of ① to ④ above, good improvement measures can not be seen at present,
    Is there a breakthrough plan?

  • Hi Ben-san,
    In the combination of PFC (UCC 28056) + LLC (UCC 256302)
    We are conducting output transient fluctuation test, but the following problem has come up.
    Please tell us about improvement measures.
     
    <Test condition>
    PFC input: AC 100 V
    LLC output: sudden change of 12 V 10 A (100%) ⇔ 0 A (0%)
    Load device: Electronic load
    Load sudden change cycle: 1 Hz duty = 50%
     
    <Problems>
    At the timing when the load has changed from 100% to 0%, the auxiliary power supply (Vcc) voltage by the LLC auxiliary winding of the evaluation board lowers and the IC operation instantaneously stops.
    After the operation is stopped, it restarts with the start circuit, but the 12 V output drops by several volts during this period. In case
    This failure phenomenon occurs at a considerable frequency.
    In case
    <Countermeasure and consideration>
    ① If 47 μF is added to the capacity of the smoothing capacitor C 16 = 120 μF of Vcc,
    The drop in Vcc was alleviated and some effect was recognized,
    Although the effect is not 100%, the drop frequency of 12 V output decreases.
     
    ② However, if this capacity 47 μF is added to the current circuit,
    The charging time of the start circuit becomes long, and it is not practical because the starting time from input power on to output rising is over.
     
    ③ As the output current range that maintains the output stability at present, the lower limit of the spec that can be compromised in sudden load change is around 0.3 A (3%), and it seems that it is necessary to add this dummy resistance.
    This will be designed to reverse from energy saving and high efficiency targets.
     
    ④ Consider setting the burst mode level for the above improvement.
    Based on the calculation formula of UCC 256304 Japanese version data sheet 8.2.2.21,
    To optimize the programming resistance and investigate whether the problem can be improved,
    Perform the following.
       When the voltage (upper limit: 1.86 V lower limit 1.14 V) measured by inserting the resistance 10 KΩ into the emitter of the photocoupler (U 2) was substituted into the calculation formula (75) of the data sheet,
    When calculated using IFb = 81 μA of the IC electrical characteristics table,
    The VLL value becomes a minus value, and the calculated numerical value has no validity, why?
     
    ⑤ From the contents of ① to ④ above, good improvement measures can not be seen at present,
    Is there a breakthrough plan?
  • Hi Doi-san,

    If VCC is dropping to 11.5V during load transient condition you can consider adjusting the turns ratio to operate at a higher VCC voltage on the bias winding. This should help avoid VCC dropout and also may render the extra VCC capacitor unnecessary. You can also adjust the burst mode threshold to make sure there are frequent enough burst packets to ensure the VCC capacitance is getting replenished frequently enough.

    I would suggest checking of the opto-coupler is saturating during no load condition and this is causing a delay in the response to the load step. You can try connecting a zener between R20 and R23 to clamp the fast lane current to prevent opto-coupler saturation. This should improve the no load to full load transient.

    Please remove R21 when you do the measurement for burst mode. R21 and D10 are sourcing current into the FB node (this circuit is supposed to help avoid opto-coupler saturation). The calculator assumes the opto-coupler current is pulled out of the FB pin and there are no external sources of current to the opto-coupler on the primary side.

    Best Regards,
    Ben Lough
  • Hi Doi-san,

    Did you get a chance to retest?

    Best Regards,
    Ben Lough
  • Hi Ben-san,

    1. In equation (67) in the UCC56301data sheet (Japanese), the share of the internal power supply share factor (Kvcrrmp) is
    The left term of the calculation formula is converted to the right term so that it is in the range of 0.1 to 0.6, and C1, Cr, Iin, Icomp
    The result can be calculated by substitution.
    However, in this right term, C2 on the lower side of the voltage divider capacitor is omitted,
    It seems as if it does not affect the setting of Kvcrrmp, but C1 = 150 pF, C2 = 0.015 μF
    What is the reason for setting range of set C2 value?

    2. As a countermeasure proposal for the problem that the output voltage drops in the previous answer mail.
    I instructed a plan to change C10 from 0.015 μF to 6.8 nF, but the implementation result was not improved.
    In our experiment, we changed the setting of C10 from 0.015 μF to 0.022 μF under the condition of R 14 = 1 MΩ,
    Load change 0% (with 1 kΩ dummy resistance between 12 V output terminals) ⇔ 100% variation,
    The burst operation at no-load is stable, and there is no drop below UVLO at Vcc,
    There was no reduction in output, and there was improvement effect.
    Is this setting reasonable? (Other evaluation board constants are default state.)

    3. From the results of the above two items, it is said that the capacity setting of the evaluation board C2 = 0.015 μF is not the optimum value in item 1
    Think about it, how can I check the optimal set values ​​of C1, C2 capacity on evaluation?

    4. With use premised on load sudden change 0 ⇔ 100%, concerning the setting of C1 and C2 capacity values ​​in 1 above,
    Please teach the proper range, or the way of thinking.

    5. No explanation about Icomp in the datasheet.Is it same as Iramp in the table?
  • Hi Doi-san,

    1. equation 67 only calculates the contribution of the internal current source. The total swing on VCR is calculated in equation 66. C2 will affect the peak to peak voltage swing on VCR. The value of C2 will affect loop response as well as the switching frequency during startup

    2. This is ok.

    3. Optimal value for VCR is dependent on your loop response (do you want higher crossover frequency or better phase margin). The capacitance of VCR will also affect the switching frequency profile during startup and you will want to make sure the startup switching frequency is fast enough to avoid tripping OCP1 but slow enough to avoid hard switching. The optimal capacitance for VCR will be dependent on the application.

    4. Typically VCR is chosen based on the measured loop response to determine if there is an adequate amount of frequency compensation for stability. Next, I would check the switching frequency profile during startup at no load as well as startup during full load. You want to make sure the switching frequency is not too low where you might trip OCP1 but also not too large to avoid hard switching during startup. You can also use the UCC25630x design calculator to help select VCR values. You can find the calculator at the bottom of this page:www.ti.com/.../toolssoftware

    5. Yes, Icomp is the same as Iramp.

    Best Regards,
    Ben Lough