Hello,
I would like to use the LMZM23600 in a board layout where the 3.3 V supply may be
- generated by the LMZM (given e.g. 8 V via an external pin)
- given via another external pin (in this case the VIN pin of the LMZM will be unpowered).
So in my layout the board has a 3-pin connector with VIN, 3.3VIN and GND, of which VIN and 3.3VIN will never both be driven in any setup.
Is it possible to simply include the LMZM23600 in this design or do I have to apply e.g. a diode?
Regards,
Nicolai