Other Parts Discussed in Thread: BQ40Z60, BQSTUDIO
7776.Battery gauge system design overview-process, flow, tools and configuration.pptxHi,
Can you please clarify the ‘Update Status going from 04 to 05 for pack side gauge’ on page 9 of the attached? seems these bits don’t line up to the register description below(??)
I plan to perform a Learn Cycle on a bq40z60.
Is the Update Status register described below the same as the one indicated on page 9 of the attached?
bqStudio/Data Memory/Gas Gauging/State/Update Status
is_Qmax_Field_Updated [3] Qmax update in the field 1:Updated, 0:Not Updated
Enable [2] IT gauging and Lifetime updating 1:Enabled, 0:Disabled
UPDATE[1:0] [1:0] Update Status 1:Detected, 0:Undetected
UPDATE[1] UPDATE[0] UPDATE STATUS
0 0 Disabled
0 1 Qmax updated
1 0 Qmax & Ra tables updated
1 1 Undefined
if i Issue an IT enable command (0x21),
then Issue a reset command (0x41),
as described on page 9 of the attached, will some of the above registers clear??
or
do i set/clear the registers manually then do the test??
Thanks,
Tom
5810.7776.Battery gauge system design overview-process, flow, tools and configuration.pptx