Other Parts Discussed in Thread: TPS55340, TPS61087, TPS61175
Hello Sir,
this is Gaurav Kothari from Mumbai, India.
we are manufacturing electronic locks which are completely battery operated (1.5V x 4 AA alkaline duracell battery). now my problem is, in our current design we are using a solonied for locking mechanism. so when the solonied gets active, we get a voltage drop of around 1V, in which sometimes our controller stop responding due to under voltage.
for example, when battery voltage is 5V, and solonied gets active, the voltage drops to 1V and controller stop responding due to under voltage, which is currently 4V. because the controller works at voltage range of 4.5V to 5.5V.
So now we are planning to use TPS61085 where we can get a constant output voltage of 5V whatever the battery voltage may be. so our circuit will be something like battery ---->> TPS61085 circuit ---->> microcontroller circuit.
so if i add TPS61085 in series between my battery and microcontroller circuit, will it keep the controller voltage constant at 5V even if the solonied gets active. The current consumption is approx 2 Amps.