This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ78Z100: BQStudio, getting started?

Part Number: BQ78Z100
Other Parts Discussed in Thread: BQ40Z50

I have designed a new battery pack using BQ78Z100.  Have successfully programmed the appropriate ChemID, but now can't figure out how to continue... the "getting started" link in software doesn't work, and the help menu is under construction.  How do I enable the pack?  What else needs to be done for the pack to be ready?  Do I have to do a relax-discharge-relax curve, even if the ChemID is found already?  Which protection settings do I need to change?  When finished with the settings, to replicate them for other packs, do I just use the firmware tab to "Read Srec from device" and load it into other packs?  

Thanks