This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM2662: 5V to +10V, and -10V 50mA

Part Number: LM2662

Dear all.

Do you have example circuit of folloing spec.
Input=5V
Output=-10V/50mA
and
Input=5V
Output=10V/50mA

Regards,
Watanabe