This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM74670-Q1: Vgs signal abnormal

Part Number: LM74670-Q1

Hi,

customer use LM74670-Q1 as full bridge rectifier, but they found the Vgs is abnormal and has noise on Vin. 

customer use 1uF as charge pump capacitor and use CSD18563Q5 as transistors. the waveform as below show.

could you help on this?

Vin is 24VAC, below is Vin wavform:

  

the Vgs waveform as below: