This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TL494: TL494- DC-DC converter -metal core constant current 200W module

Part Number: TL494

Hello friends. I want to make an output in this PWM so that dc dc conwerter I can control it using a microcontroller. Does anyone know how?

  • Hello Rafal,
    You should review the design references on the webpage for the TL494.
    For example Figure 35 in this document :
    www.ti.com/.../slva001e.pdf
    shows how to control the output voltage of a particular DCDC converter that has a fixed voltage output with current limit.
    You can use this as a basis for design ideas on how to implement you system requirements.
    When you have more information on your requirements you will be able to proceed with an actual circuit design.

    Regards
    John