Other Parts Discussed in Thread: BQ24172
Hello,
After doing the learning cycle at 4.2V with bq27510-g3 gauge, what are all the parameters to be modify before generate the golden image ?
I suppose change
Configuration : CC Threshold, Design Capacity, Charging Voltage 4100mV
Should I change :
Gas Gauging,"State","Qmax Cell 0"
Gas Gauging,"State","Qmax Cell 1"
Gas Gauging,"State","Cell 0 V at Chg Term","4100","mV"
Gas Gauging,"State","Cell 1 V at Chg Term","4100","mV"
OCV Tables,"OCVa0 Table","Qmax Cell"
OCV Tables,"OCVa1 Table","Qmax Cell"
?
Are there other parameters ?
Do you have some documentation that explain the step between learning cycle at 4.2V and golden image generation for 4.1V system ?
Thanks
Stéphane