Other Parts Discussed in Thread: UCC25600,
I need to design a cost-effective battery charger with an output capability of 11-15 volts at up to 40 amps (600W). This application uses an input of 105-130 volts ac and does not need PFC.
1. The UCC25630-4 looks like a good choice, although TI recommends it for 75 W to 500 W. I’ve looked at TIDA-01501 (700 W) which seems to stretch this a bit. What are the caveats and the cause of the power limit? Can it be scaled up for higher power (600 W to 1200 W) – maybe using gate driver ICs? (I would also like to consider a version that can provide 1 or 1.2 kW.) Which gate driver IC would you recommend for a higher power application?
2. Are there any app notes about the best way to implement microprocessor control of output voltage and current limit (using D/A outputs)? I would like to be able to drop the output voltage to a lower level to implement a battery charging profile, and possibly foldback current-limiting.
Thanks,
Mike