This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28070: Adopt Current Sense Resistor instead of CT.

Part Number: UCC28070

Hello Team,

My customer intend to use UCC28070 but they don't like CT. So

1. Can they use Current Sense Resistor instead of CT?

2. If yes, should they place Rsense at MOSFET source to gnd? is that correct?

3. In order to reduce power losses of Rsense, they intend to use low Ohmic value Rsense so they will have to set PKLMT at 0.5V~1V as power limit threshold, can they do that? any potential risk?

Thanks,

Martin