Other Parts Discussed in Thread: UCC28060, , UCC28063
Can you please help clarify what value or range of values is appropriate for RTSET and how that is determined? The UCC 28046 Design Calculator spreadsheet gives a value, but that value is related only to Eq (45) of the datasheet for RTH, but does not give a value for RTL, which in most cases (?) is the stated result when solving Eq (44) for RT = min(RTH, RTL). More confusing, the example of section 9.2.2.9 in the datasheet says the value chosen for RT is 91K, but that is not even close to the result of Eq. 44 for the values given in the example, and instead should be more like 68K. The example also seems to follow the UCC28064EVM board requirements, but the eval board has 115K loaded for RT == R15. Following the WEBENCH example did not help either, as it yielded yet another value of 88.7K that didn't seem to change when I changed the value of the inductor, even after I plugged the same values that were relatively close to the datasheet requirements/results in. So what exactly is the right equation or method for determining the correct value or range of values for RTSET?
Jim