Part Number: LM9036
Other Parts Discussed in Thread: LM2936, , LM78L
Is the internal architecture for LM9036 is similar to LM2936? Does the LM9036 has resistor divider at the output for voltage feedback?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Eric,
For example consider the application as below. Because of the internal resistor divider, the LDO output is no longer regulated to fixed voltage in case of LM9036 and LM2936. However, LM78L05 regulates to fixed voltage in the same application. I am looking for a high voltage part (40V min) to replace LM78L05. Is the feedback is actual output in LM78L05 instead of resistor divider?
Regards
Murali