Other Parts Discussed in Thread: LM5160, LP2952-N, LP2953
In addition to my previous question I would like to know if TI has an LDO which meets the same requirements.
You can find the question here:
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Gerard,
thanks for your reply! What about an LDO with a sink/supply capability of 300-500mA each? And how much current can these LDOs sink that you mentioned?
I also thought of a LM7812/LM7912 combination or newer counterparts using one as the current source and the other as the current sink.
Hi Cienski,
I apologize for a mistake in my earlier post. TI does have offer the LP2953 and LP2952-N LDOs with active output discharge that support 24 V input and 12 V output. The current sinking capability is 50 mA typical, and the device must be put in shutdown mode first to sink any current. Keep in mind that with a maximum of 3 W power dissipation , the PCB will have to be optimized for thermal performance to prevent the regulator from entering thermal shutdown.
Regarding negative output regulators - although current does travel from output to input, it's the input supply that will be sinking the current, not the LDO. If you are actually looking for negative rail LDOs that support a 300-500 mA load, TI has a wide selection. You can use the LDO parametric search on the TI website under the Products tab here:

Thanks,
Gerard