Part Number: TPS23750
Other Parts Discussed in Thread: TPS23753A
We are using the TPS23750 as a non-isolated design with 12.5 VDC of output power. We are also using auxiliary power of the device using ORing Option 3 (the power going directly to the output side of the PoE power converter).
If I am powering the device with just the aux power, everything works fine until I bring the voltage up to 12.8 V in which there is a 30 mA jump in current. I also have one of the TPS23750 eval boards and I am seeing this same jump in current right around 12.8 V.
A few questions:
- Is there a maximum Voltage that is allowed to power from Aux power if using ORing Option 3?
- Do I risk damaging my PoE Circuitry if I power the device externally with 13 VDC?