This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC2895: Can I sync down in frequency?

Part Number: UCC2895


Hello,

I would like to use the UCC2895 with the timing resistor and capacitor (RT, CT) set at constant switching frequency. Would it then be possible to use the SYNC input pin to apply a clock of a lower frequency?

Thanks!

Reed Kaczmarek 

  • Hello Reed

    The UCC2895 will Synchronise only to a higher frequency than that set by the RT,CT components. Attempting to synchronise to a lower frequency will result in unpredictable behaviour and probably cause damage to the power components.

    The UCC28950 may be synchronised up or down from the frequency set by its timing resistor, additional details are in the datasheet.

    Regards
    Colin