This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV62568A: Soft start time of TLV62568A

Part Number: TLV62568A
Other Parts Discussed in Thread: TLV62568

Hi

I have a question about soft start time of TLV62568A.
This device's typ soft start time is 0.9ms in "6.5 Electrical Characteristics".
Could you tell me Cout value at this soft start time?

Best regards,
Yokota
  • Hi

    I'm sorry but please let me ask you more question.
    As long as I read the figure 21, there are delay time(about 200us) by starting soft start after high EN.
    Are there the specific value about this delay time?

    Best regards,
    Yokota
  • Hi Yokota,

    the 0.9ms is the timing of the internal reference circuit. this is not tested in an application environnement. This includes the delay time ( about 200us) and the ramup until 95% of Vou is reached.

    thanks
    Sabrina
  • Hi Sabria-san

    Thank you for the information.
    Could you tell me the Cout value at tss(typ)=0.9ms in  "6.5 Electrical Characteristics"?

    Best regards,
    Yokota
  • Hi Yokota-san,

    The softstart time tss is check within one of the implemented test-modes in production. During this test-mode the Cout values does not play a role, because the internal ramp of the voltage reference is independent of any external parameters.

    For the typical softstart time of tss = 0.9ms the recommended output voltage range - as in the datasheet mentioned - is covered as long as the output load does not drive the TLV62568/9 in overload condition above the specified max load condition.

    Could you please tell me why is this parameter critical? how is it affecting the application
  • Hi Sabrina-san


    Thank you for the reply.
    My customer have a possibility using Cout beyond recommended value.
    So they worry about whether tss will change depending on Cout value.

    Best regards,
    Yokota
  • Usually we recommend not to go above the recommended output capacitance for the  control toplogy of this device. What Cout customer wants to use? is it to power an FPGA?

    Could you precise the operating conditions ? Vin, Vout Iout (including load profile)

  • Hi Sabrina-san

    The condition is Vin=3.3V, Vout=1.2V and Iout=300~600mA
    The load is DDR and CPU.
    They will use Cout 10uF + 22uF(Bypass capacitor).

    Best regards,
    Yokota