Part Number: TLV62568A
Other Parts Discussed in Thread: TPS62088, TPS62843
I couldn't find a specification in the component's datasheet specifying the output voltage tolerance/accuracy of the converter. The only mention of "accuracy" relevant to the converter's output is the mention that reducing the resistance of the feedback network increases "output voltage accuracy but increase current consumption." The current consumption is not an issue however I need the converter to output 1.1V within +-4%.
Is there a way to guarantee this converter will perform within the 4% spec?
Thanks, Nate