Hi,
Adding on to the query raised in the thread (http://e2e.ti.com/support/power-management/f/196/t/680230.)
Can I use the VREF 3.3V output voltage as pull up voltage for the TS, STAT1, STAT2, PG# open drain pins , along with the MODE, CE as well as ISET2 pin? Because my input voltage( external adapter ) is 12V
and absolute maximum for the TS, STAT1, STAT2, PG# , MODE, CE and ISET2 is 7V so i cannot pull it up to Input voltage
So confirm on that i can use VREF pin for the pull up purpose, also please suggest what pull up resistor value should i use for this?
Regards,
Karthik