This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ78Z100: Can we use BQ28z610 as a drop-in replacement?

Part Number: BQ78Z100
Other Parts Discussed in Thread: BQ28Z610

Hi there,

   We use BQ78Z100 in a 2-cell battery pack. But the part lead time is very long which can not meet our build schedule.

  We are seeking an alternative by using BQ28z610 as a replacement.

  Can the BQ28610 be a drop-in replacement for our application below?

Single cell:   3.8V nominal and 2980mAh

Cell configuration:  2 series LI-ion cell (2S1P)

Norminal voltage (2S1p): 7.6V

Protection: same as BQ78z100

Communication: I2C 400KHz

Authentication Required:: SHA-1

Production software: Battery Management Studio

Leo