Other Parts Discussed in Thread: BQ78350
Hi,
I brought up an issue I had a while ago where I asked how to incorporate the supply current of the AFE and Gauge (18mA) into battery discharge in order to preserve the accuracy of the gas gauge. The reply stated that I could incorporate it into the self-discharge of the battery and that it should be negligible. Maybe my math is wrong but 18mA does not seem to be a negligible value. We are using an 11000mAH battery. At 18mA the battery will drain in about 25 days. The Lithium ion is about 0.1% a day self-discharge which should be 1000 days to fully self-discharge. Am I doing something incorrectly in this calculation? It seems as if the electronics will incur a 4% discharge everyday. Even though it's negligible for a discharge cycle, it isn't negligible for storage. How can I deal with this issue.
Thanks,
JP