This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27441-G1: Battery guage error

Part Number: BQ27441-G1

Hi Friends,

I have few clarification regarding bq27441-g1A

1) Other then changing cc_gain how else I can configure bq27441-g1A as 10Ah battery guage.

2) When power supply is connected and battery is inserted Power on reset is occuring and I can check it by reading the flag register

So I will go to configure the guage by 8000mAh configuration but after that inspite of having less remaining battery capacity

remaining battery capacity and Full Charge Capacity showing the same value which is the maximum value.

But if I just insert the battery other then the power supply It shows the real value of remaining battery capacity.

What condition should be satisfied or where can I get schematic reference for battery guage which satisfies chargable battery.

Regards

Harish