Hi,
I am designing a Battery Operated Low Power Device, battery used will be of 3.6V Li-Po. TPS63031 is used as a buck boost converter. I have designed a custom PCB for the project.
During Initial Tests, the TPS63031 was showing a current consumption of 40uA at no load, which is approx similar to quiescent current in datasheet specs. But after I connect a micro controller and an LED, the current consumption measured is quite high and unstable ranging between 250uA to 120 uA.
Points to note,
1. The micro controller is put in to low power sleep mode, making the PSCTL Pin of TPS Low to enter power save mode.
2. During Run Mode of Micro controller, PSCTL Pin is pulled high to disable power save mode.
3. The measured current test values always differ for different attempts.
For reference I am attaching the circuit schematic pdf of TPS63031.
Thank You,
Amit Kotal