Other Parts Discussed in Thread: UCC28951,
Hi
Currently my customers are developing 600W class solar converters using SM72445 and UCC28950.
The configuration is as follows.
The company is trying to apply ucc28950 as a boost circuit.
Input: 48V, Output: 400V, Input maximum: 600W
Could you please review the circuit diagram below?
PSFB_Controller_schematic.pdfPSFB_Power_schematic.pdf
I am currently in the process of reviewing the circuit schematic. I am busy, but can you help me?
I did not see the use to Boost Output, including me.
If it is 600W class, can it be configured as LLC IC?
At the customer company, it is said that the efficiency is not good when the input voltage moves when constructing the LLC. Is it true? I also heard that resonance is difficult to apply.
I think UCC25630X is also applicable if LLC is applicable.