Other Parts Discussed in Thread: BQ25890
Hi,
if charge battery is not full, i hope battery could up to 96~97% full.
Not just 92% full,
but BQ24610 is not only from 92% nearly full and really slowly charging ,but also stop at 92.5%,
is this correct?
Q1: How could i cheat BQ24610 for charging up to 96~97%(the new battery could arive really)
,and how could i let nearly full charge time be not so long,
i hope if fast charge state current is limit at 2A, and i think nearly full state current should be 0.2A,
but the truth is every 1mA by charing every two minute.
Q2: Could i let BQ24610 be more fast when nearly full?
--------------------------------------------------------------------------------------------------------------------------
Circuit is all the same with the application of datasheet .
Below is what i had tried and detected:
1. i have change from R1 100K to 91k , but STAT1,2 change to high and high, that mean i can't cheat BQ24610 with Vfb.
2. R2 from 500k to 560k , the same result above.
If i could't cheat with Vfb,what other way could i try?