Other Parts Discussed in Thread: BQ25703A
1. VBUS=0V,
Valid battery voltage is set REG0x15()
OTG output voltage is set in REG0x3B() and output current is set in REG0x3C()
EN_OTG pin is HIGH and REG0x32[12] = 1
VBUS is belowVVBUS_UVLO
10 ms after the above conditions
OTG start failed,
which other conditions will affect the OTG Converter starts?
2, 3cells battery configuration, can we set charge voltage 13.2V or higher?
thanks
BR
Jelly