This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ78350-R1: Understanding the "accumulated change in capacity" for valid charge termination

Part Number: BQ78350-R1

Hi Based on the criteria for VTC:

All of the following conditions must occur for two consecutive 40-s periods: Charging (that is, BatteryStatus[DSG] = 0) AND AverageCurrent() < Charge Term Taper Current AND Max (CellVoltage1..15()) + Charge Term Voltage ≥ ChargingVoltage()/number of cells in series AND The accumulated change in capacity > 0.25 mAh since current and voltage termination conditions where first detected.

I was wondering if it is supposed to be the "The accumulated change in capacity < 0.25 mAh". I just thought that it would check to see if it's "slowing down" or not increasing capacity, so anything under that limit would be regarded as the battery being at full to almost full capacity. Am I interpreting it correctly? Can you help me with this one?

JP