Part Number: TPS61089
Hi,
I'm going to use TPS61089 to realize these 3 condition:
1) Vin=4,5V, Vout=6V, Iout =1A (continuos)
2) Vin=4,5V, Vout=12V, Iout =1A (continuos)
3) Vin=4,5V, Vout=12V, Iout =2A (continuos)
For the first and second option I think there is no problem! Right?
But for the third option, should I have some problem? Datasheet and evaluation board tested the TPS61089 with Vout =9V and Iout =2A, but with Vout =12V can I reach safely 2A of current with acceptable ripple and efficiency?
Thank you in advance for replay