Other Parts Discussed in Thread: TPS40210, TPS43061, PMP9772, TPS61088, TLV61220
Hello,
I am designing a boost circuit using the IC TPS61089 Parameters of the circuit are mentioned below :
1)Input parameters = batttery powered rated 4.7v 7000mAH 1C discharge rate.Min Vin(min)=3.3V.
2)Output Parameters = Vout=12v and Iout=4.5A.
Below is the schematic that i have designed is this design correct as per my output parameters or any changes are there.
I tried to simulate the circuit in the web-bench tool but not getting results.
So Kindly provide solution as per the output parameters...!!!