This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24610: Issue with the Charging for the BQ24610

Part Number: BQ24610


Hello,

I have been a bit confused on the charging of the BQ24610 with the STAT 1 and STAT 2 pins and how it should turn-off charging when it completes.

My battery which is a 5S1P has a cut-off about 21.5-21.6V.

But the BQ24610 seams to continue chraging, when it reached 21.6V, voltage now jumps around between 20.6V to 21V and also the STAT1 LED which was solid ON when charging now flickers on every 3 seconds.

The voltage limiting resistors are set  for R25=909k and R28=100K as dictated by the sluu396a datasheet for the BQ24610 EVM.

Would it be possible to have some help and advise on how to fix this?

Best regards

Mo