Part Number: BQ24125
Hello,
The calculations for Riset2 (equation 18 on page 24 of bq24125 datasheet) state that:
Kiset2 = 1000 (confirmed in datasheet)
Rsns = from my schematic, e.g. 0.5 ohms in my case
Icharge = the fast charge current correct? In our case it would be 200mA.
Where is Viset2 defined? Datasheet mentions 100mV (Precharge set voltage, ISET2, on page 6) BUT, the example in the datasheet (again, equation 18) uses 1.0.
For this board, Riset1 = (Kiset1 * Viset1 ) / (Rsns * Icharge) = (1000 * 1) / (0.5 * 0.2) = 10k
I have the board running, and have verified that I'm getting 0.2A with the 10k Riset1 value.
But I don't have a way of verifying Riset2 without waiting for the whole charge cycle to complete, and that's like watching paint dry.