This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24171: The charging current of BQ24171 battery is 3A at 3.3V. But when the battery is charged to 3.8V, the charging current is only 200 mA.Is there a problem with the circuit?

Expert 2630 points
Part Number: BQ24171

The charging current of BQ24171 battery is 3A at 3.3V. But when the battery is charged to 3.8V, the charging current is only 200 mA.Is there a problem with the circuit?BQ24171.pdf