This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: TINA-TI or Spice Models
Hello,
I tried to use the LM4041 in a third party SPICE simulator. Therefore I have used the unencrypted models from this web page below.
Unfortunately all the unencrypted models let fail the simulation in every SPICE-simulator, if the Anode of the LM4041 is not connected to GND.
The reason is that there is a mistake in the model file (.lib) at one referenced voltage in the line below.
E_Estart ..... V(Q20B)...
This mistake will automatically reference this V(Q20B) to GND (net 0) instead of "V-". If the anode of the LM4041 isn't connectd to GND, the simulation will fail.
This line should be corrected to
E_Estart ..... V(Q20B,V-)...
Could you pleaes correct this mistake in all the unencrypted model files (.lib) from this web page.
Helmut
Hi ,
You can try to simulate latest revised model of LM4041_NA1P2.
LM4041-NA1P2 PSpice Transient Model (Rev. A)
Please let me know if you are still facing the same issue.
Thanks & Regards,
Saket