I have been trying to determine the output frequency from using the formula that is in the datasheet and it does not work out to what I have bread boarded. Is there a different formula to determine the output frequency. Could it have anything to do with the voltage. I'm using 15VDC as input voltage. I have 102nF cap and 100K resistor. What should my output Freq be?