I would like to directly drive an LED, if possible, at about 1mA when the regulator outputs are operating normally. e.g. wiring +12V through 10K to the LED anode and then connecting the LED cathode to the PGOOD pin of the LM27762. Will this be OK or do I need to add something else to drive the LED instead? (e.g. base/gate of transistor)