Hello
1. What are the minimum conditions to obtain PWM on pins 17-22?
2. I am doing an experiment on this IC and let me explain the setup. I am giving PWM to full bridge inverters by using microcontroller and gate drivers so that I can vary DUTY CYCLE. On the secondary side of the transformer I have placed full bridge diodes instead of Syn Rectifiers for easier understanding. Later I give the main feedback signals of VOUT and Input current via Current sense transformer. Atleast I am expecting PWM on all the pins (17-22). But I observe PWM only on pins 19-22 with 50% duty cycle. The output voltage is well within the design range. Where am I going wrong?
3. Will I get PWMs if I give DC less than 2V on CS channel (pin 15) provided I have given DC less than 2.5V on pin 3?