Hello;
Can you please clarify how the COMMx lines should be connected when they're not used? i.e. do I need to add termination R's as implied in 8.1.2.1 (assuming it's not referring to the internal R's)?
The programing guide says I can
8.1.2.1 Single-Ended Communication (UART)
Communication with the bq76PL455A-Q1 from a host controller is performed utilizing a UART communication
protocol. The UART interface requires the following configuration:
1. COMML- is connected by 100-kΩ pull-down to DGND.
2. COMML+ is connected by 100-kΩ pull-up to V5VAO.
8.1.2.2.8 Unused Differential Communications Pins
Unused stack communications pins (COMMH+/–, COMML+/–, FAULTH+/–, FAULTL+/–) have internal
terminations; no external pull-up or pull-down resistors are required on these pins, if not used. If not used, leave
the unused pins unconnected. The COMMH drivers cannot be disabled.
...yet the Software design reference says: (SLVA617A)
1.2.5 Disable High-Side Receiver on Differential Interface on Top of Stack
To reduce current consumption and turn off the receipt of undesired messages due to noise from
nonexistent boards above the top-most device, this message turns off the high-side differential receiver
interface on the bq76PL455A-Q1 device at the top of the stack (bq76PL455A-Q1 at Device Address 1 in
this example). Specifically, this message clears the COMM_HIGH_EN bit in the Communication
Configuration register (address 16 to 17) on the top-most device in the chain