This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2491: Behavior of PG pin

Part Number: TPS2491

Dear Specialists,

My customer is considering TPS2491 and has a question.

I would be grateful if you could advise.

---

I confirmed the behavior of the PG pin and have three questions.

Could you please see attached schematic and waveform.

question about PG pin .pptx

---

I appreciate your great help in advance.

Best regards,

Shinichi

  • Hi Shinichi,

    I will go through the test waveform and clarify.

    Best Regards,
    Rakesh
  • Hi Shinichi,

    During startup, PG output depends on VDS of external FET. The VDS has to fall below 1.25 V and then wait 9ms (typ) to assert PG output HIGH.

    During an fault, the device goes into protection mode and VDS increases. Once VDS increases above 2.7V, the PG output goes LOW after 9ms (typ) deglitch time.
    In case, device is disabled by doing EN < EN_L, the PG output goes LOW after 9ms (typ) deglitch time.

    Refer Section "7.3.9 PG" in the datasheet and let me know if there are any further questions.

    Best Regards,
    Rakesh
  • Hi Rakesh,

    Thank you for your reply.

    I understand PG output depends on VDS of external FET, not EN and Vccc.

    I'll share this information with the customer.

    I appreciate your great help.

    Best regards,

    Shinichi