This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5143-Q1: Inductor value calculation is differs from the LM5143-Q1 quickstart calculator compared to using datasheet calculation

Part Number: LM5143-Q1


The Quickstart calculator shows significant different inductor value compared to using datasheet equation 15 calculation.

Input: 48V      Output: 42V, 20A   Fsw = 500 KHZ

Buck Inductor value using equation 15: 

1.75uH

From the LM5143-Q1 quickstart calculator:

Ch1 Recommended Inductance: 10.5uH

The quickstart calculator:seems to be high.