Part Number: TPS65217
Other Parts Discussed in Thread: TPS54424
Hello,
I am creating a custom device based on the BeagleBoard Black which uses the TPS65217C power management chip.
The device needs to be powered by a 12V unregulated supply with tolerance for 10V - 14.5V. The TPS65217C datasheet indicates it can support a supply voltage range of -0.3V to 20V, however, the recommended operating supply voltage is 4.3V - 5.8V. Can the TPS65217C be powered directly by the unregulated 12v power source without any issues?
Thank you in advance